/*** 
This is the menu creation code - place it right after you body tag
Feel free to add this to a stand-alone js file and link it to your page.
**/

//Menu object creation
oCMenu=new makeCM("oCMenu") //Making the menu object. Argument: menuname

oCMenu.frames=0

//Menu properties   
oCMenu.pxBetween=0
oCMenu.fromLeft=5 
oCMenu.fromTop=60   
oCMenu.rows=1 
oCMenu.menuPlacement="left"

oCMenu.openOnClick=1                                                            
oCMenu.offlineRoot="" 
oCMenu.onlineRoot="" 
oCMenu.resizeCheck=1 
oCMenu.wait=700 
oCMenu.fillImg="http://www.rockwellautomation.com/lib/images/cm_fill.gif"
oCMenu.zIndex=500

//Background bar properties
oCMenu.useBar=0
oCMenu.barWidth=640
oCMenu.barHeight=17
oCMenu.barClass="clBar"
oCMenu.barX=0
oCMenu.barY=63
oCMenu.barBorderX=0
oCMenu.barBorderY=0
oCMenu.barBorderClass=""

//Level properties - ALL properties have to be spesified in level 0
oCMenu.level[0]=new cm_makeLevel() //Add this for each new level
oCMenu.level[0].width=185
oCMenu.level[0].height=17 
oCMenu.level[0].regClass="clLevel0"
oCMenu.level[0].overClass="clLevel0over"
oCMenu.level[0].borderX=0
oCMenu.level[0].borderY=0
oCMenu.level[0].borderClass="clLevel0border"
oCMenu.level[0].offsetX=8
oCMenu.level[0].offsetY=0
oCMenu.level[0].rows=0
oCMenu.level[0].align="bottom"

//EXAMPLE SUB LEVEL[1] PROPERTIES - You have to specify the properties you want different from LEVEL[0] - If you want all items to look the same just remove this
oCMenu.level[1]=new cm_makeLevel() //Add this for each new level (adding one to the number)
oCMenu.level[1].width=185
oCMenu.level[1].height=17
oCMenu.level[1].regClass="clLevel1"
oCMenu.level[1].overClass="clLevel1over"
oCMenu.level[1].borderX=1
oCMenu.level[1].borderY=1
oCMenu.level[1].align="right" 
oCMenu.level[1].offsetX=-8
oCMenu.level[1].offsetY=2
oCMenu.level[1].borderClass="clLevel1border"
oCMenu.level[1].arrow=""
oCMenu.level[1].arrowWidth=13
oCMenu.level[1].arrowHeight=9
oCMenu.zIndex[1]=200

//EXAMPLE SUB LEVEL[2] PROPERTIES - You have to specify the properties you want different from LEVEL[1] OR LEVEL[0] - If you want all items to look the same just remove this
oCMenu.level[2]=new cm_makeLevel() //Add this for each new level (adding one to the number)
oCMenu.level[2].width=185
oCMenu.level[2].height=17
oCMenu.level[2].regClass="clLevel2"
oCMenu.level[2].overClass="clLevel2over"
oCMenu.level[2].align="right"
oCMenu.level[2].offsetX=-5
oCMenu.level[2].offsetY=0
oCMenu.level[2].borderClass="clLevel2border"
oCMenu.level[2].arrow="lib/images"
oCMenu.level[2].arrowWidth=13
oCMenu.level[2].arrowHeight=9
oCMenu.zIndex[2]=200