DOWNLOAD the Performance level calculator

The SISTEMA tool automates calculation of the attained Performance Level from the safety-related parts of a machine’s control system to EN ISO 13849-1. Data for Rockwell Automation machinery safety products is now available in the form of a library file to be used with the SISTEMA calculation tool. The combination of the two gives machinery and system designers comprehensive time-saving support in evaluating safety to EN ISO 13849-1.

To download the software click here